- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Disable touch and key input for an alarm table
Disable touch and key input for an alarm table to prevent interaction with the table on the HMI device. For example, disable touch and key input for an alarm table to prevent selecting alarms on the HMI device.
To disable touch and key input for an alarm table
- On the screen, select the alarm table.
- In thePropertieswindow, select thePropertiestab.
- Expand theAppearancenode.
- ClearEnabled.
Provide Feedback