- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Copy a Security Administration user account
Copy a Security Administration user account to reuse the information within and across
View Designer
projects. Copy individual items from the user account or copy an entire user account card including the password and PIN.Prerequisites
- Open the sourceView Designerproject containing the content to copy.
- If the content is to be pasted into another project, for each project, start an instance ofView Designerand open the target project. It is recommended to open no more than three instances ofView Designerat one time.
To copy a Security Administration user account
- In the source project, selectTools > Security Administration.
- Select theUserstab to display theUser Accountsbox.
- In theUser Accountsbox, select a user account card, and then right-click and selectCopy.
- To copy a single item, highlight the item, and then right-click and selectCopy.
- In each target project in theUser Accountsbox, select a card (outside of theUser Namebox), right-click and selectPaste. The card pastes below the currently selected card.
- If a new user card is selected, the card pastes above it.
- To paste a single item, right-click the appropriate box on the user account card and selectPaste.
- SelectOKto apply the changes and close the dialog box.TIP:Tips:
- Copy only one user card at a time.
- A red outline around a box on a user account card indicates an error condition, such as a duplicate name or PIN. You must correct all errors before you can save the changes.
- Cut aSecurity Administrationuser account by selectingCutinstead ofCopy.
Provide Feedback