- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Set security
View Designer
security provides the ability to control access to the runtime application by controlling access to: - The HMI device
- Individual screens, shortcuts, and popups
- Graphic elements
- Downloads to the HMI device
Security is project-specific, not application-wide, and applies only to user (role) runtime access.
Use the
Security Administration
dialog box to set up access rights for anyone interacting with the HMI device.Provide Feedback