Log On Method tab

Log On Method tab

How do I open the HMI Device tab?
On the
Menu
bar, click
PROJECT > Project Properties
and click the
HMI Device
tab.
Use the
Log On Method
tab on the
Project Properties
dialog box to specify how users log on to the HMI device. You can require users to log on with a user name and password, or with a PIN.
Use the
Security Administration
dialog box to specify the password and/or PIN for each user.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.