- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
System Banner
The
System Banner
appears at the top of each screen configured to show the banner. If a screen is configured to show the System Banner
, shortcuts to that screen show the banner. The System Banner
contains a default set of items. Display the
System Banner
on screens to log on and off, navigate to screens, and display network and controller issues on the HMI device. Change the System Banner
by changing its height, background color, and contents, or removing the System Banner
. Provide Feedback