- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Close all screens
Close all screens in a project simultaneously to not close each screen individually. Closing all documents closes only screens. All other windows and tabs remain open.
To close all screens
- SelectWindow >Close All Documents.
- If prompted to save changes to the screens, selectYesto save changes, or selectNoto not save changes.
Provide Feedback