Work with screens

Work with screens

Use a screen to contain content and create shortcuts that appear in the application on the HMI device. After adding a screen to a project, build the content and design the behavior to see on the HMI device. A
View Designer
project for a PanelView 5310 can contain no more than a total of 100 screens and popups. A
View Designer
project for a PanelView 5510 can contain no more than a total of 500 screens and popups. Projects must have a minimum of one screen.
Once the screen is created, add content to and configure the behavior of the screen to provide interactivity on the HMI device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.