- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Rename a screen
By default, each project contains a screen named Screen_001. This number increments with each new screen created with the same name.
Rename a screen to make the name more meaningful. For example, give the screen a name that reflects its purpose, content, or targeted use. Names within a folder must be unique and are not case sensitive. For example, Bottling_Line and bottling_line are considered identical names. Renaming any screen in the
Predefined Screens
folder is not allowed.To rename a screen:
- In theProject Explorer, expand theUser-Defined Screensfolder.
- Click the screen once to select the item.
- Click the screen again and type the new name.TIP:Right-clicking the name, selectingRename, and entering a new name also renames the screen.
Provide Feedback