Delete a screen

Delete a screen

Delete a screen to remove it from the project. Delete screens from the
User-Defined Screens
folder in the
Project Explorer
. To delete a screen that is referenced by shortcuts, first delete the shortcuts. Deleting a screen from the
Predefined Screens
folder is not allowed. You cannot undelete a screen.
Prerequisites
  • In the
    Navigation Menu
    folder, delete any shortcuts based on the screen to delete.
To delete a screen
  1. In the
    Project Explorer
    , expand the
    User-Defined Screens
    folder.
  2. Right-click the screen, and select
    Delete
    . The screen is removed from the
    Project Explorer
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.