- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Create a screen
A screen in
View Designer
contains the items to appear on the screen on the HMI device. After adding a screen to a project, build the content and design the behavior to see on the HMI device. A View Designer
project for a PanelView 5310 can contain no more than a total of 100 screens and popups. A View Designer
project for a PanelView 5510 can contain no more than a total of 500 screens and popups. Projects must have a minimum of one screen.To create a screen:
- In theProject Explorer, right-click theUser-Defined Screensfolder and clickNew Screen. A screen named Screen_002 or increment number is added to the folder.
TIP:
After adding the screen, create content for it by adding graphic elements.
Provide Feedback