Configure the HMI device

Configure the HMI device

The
Settings
screen contains options to setup the HMI device, network, display, and controllers.
Use the
Settings
screen to configure the HMI device and view network diagnostics. If the HMI device is in error, collect additional troubleshooting data. For more information about configuring the HMI device, refer to the
PanelView 5310 Terminals User Manual 2713-UM001
and the
PanelView 5510 Terminals User Manual 2715-UM001
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.