Activate the VNC server at runtime

Activate the VNC server at runtime

Use the VNC screen to activate or de-activate the VNC server.
To Activate the VNC server
  • Select an access command:
    • VNC View-Only Access - View content on the HMI device only.
    • VNC Full-Control Access - View content and interact with the HMI device.
    • Disable VNC Server- Disables the VNC server.
      TIP:
      Use
      View Designer
      to configure access rights for users remotely connecting to an HMI device.
NOTE:
After rebooting the PanelView 5000 HMI device, the VNC server configuration automatically resets to the Disabled state.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.