- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Equipment Phase Properties dialog box - Configuration tab
How do I access the
Equipment Phase
Properties dialog box?
In the
Controller Organizer
or Logical
Organizer
, right-click an <EP>
and select
Properties
.Use the
Configuration
tab to set up specific behaviors for the equipment phase, configure which routines to use for the Prestate and Fault routines, and, if the equipment phase input tags are used in an Equipment Sequence
, determine how values are assigned. Do these tasks on the
Configuration
tab.- Choose the routines to use with thisEquipment Phasefrom thePrestateandFaultlists.
- Inhibit the controller from executing thisEquipment Phase.
- Synchronize data at the end of the phase execution.
- Choose the state to which the system should initialize theEquipment Phase.
- Signal the completion of a state any time the equipment phase transitions to a state where the state routine is not implemented.
- Enter an initial value for the step index.
- Choose the action to take if communication with an external sequencer fails.
- Choose the action to take when an external request initiated using the PXRQ instruction is in progress and the equipment phase receives a HOLD command (while in the RUNNING state).
- Assign phase inputs and outputs when used in anEquipment Sequence.
Provide Feedback