- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Routine Display
The
Ladder Editor Routine Display
illustrates the elements that make up the ladder diagram logic routines. To enter ladder logic, drag the ladder elements from the Ladder Instruction
toolbar and drop them into the Routine Display
. The Ladder Editor Routine Display elements may include:- rungs
- branches
- instructions
- operands
- instruction comments
- main operand tag descriptionsTIP:When entering instructions the question mark symbol (?) is used to denote where to enter a value for the instruction.Two question marks (??) display when the value should be supplied by the system, but the system was unable to attain the value.
Provide Feedback