Delete a Routine

Delete a Routine

Delete a routine to remove it and all its ladder logic from a program.
IMPORTANT:
If the routine to delete is the Main routine or Fault routine of its program, first edit the program properties to disassociate the routine from its function in the program.
To delete a routine
  1. Select the routine to delete.
  2. Press the
    Del
    key.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal