Create a key value converter

Create a converter that changes Boolean values into localized text.
  1. In the
    Project view
    pane, right-click
    Converters
    and select
    New
    Key-value converter
    .
  2. Double-click the converter.
  3. In the central pane, set the following values:
    Keys
    Boolean
    Values
    String
    True
    True
    False
    False
    For more information about dynamic links, see Create dynamic links.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.