Create an event logger

Create an event logger

Create a logger that monitors the current temperature.
  1. In the
    Project view
    pane, right-click
    Loggers
    and select
    New
    Event logger
    .
  2. Configure events:
    1. In the
      Properties
      pane, next to
      Event configurations
      , select
      Add
      .
    2. Set the
      Listen subtree
      property value to
      False
      .
    3. Set the
      Event type
      property value to
      AlarmConditionType
      .
    4. In the
      Properties
      pane, double-click
      EventLogger1
    5. In the central pane, select these variables:
      • BaseEventType
        Message
        .
      • BaseEventType
        Severity
        .
      • BaseEventType
        Time
        .
      • BaseEventType
        ConditionType
        AcknowledgeableConditionType
        AckedState
        Id
        .
      • BaseEventType
        ConditionType
        AcknowledgeableConditionType
        ConfirmedState
        Id
        .
      • BaseEventType
        ConditionType
        AcknowledgeableConditionType
        AlarmConditionType
        ActiveState
        Id
        .
    6. In the central pane, select
      Apply
      .
  3. Create a dynamic link between the
    Database
    property and
    ProjectName
    DataStores
    EmbeddedDatabase1
    .
    For more information about dynamic links, see Create dynamic links.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal