Create a check box that shows or hides clock
Create a check box dynamically linked with a user-specific variable that shows or hides clock.
- Create the check box:
- In theProject viewpane, right-clickMainWindow (type)and select .
- Hover-over the check box, select, and enterShowClockCheckBox.
- Configure the check box:
- In thePropertiespane, create a dynamic link between theActiveproperty and .For more information about dynamic links, see Create dynamic links.
- Set theTextproperty value toShow clock.
Fornire un feedback