Develop a persistent setting specific to a user

Create a check box that shows or hides a clock label, which state is persistent based on the currently logged in user.
Application example
NOTA:
Download the sample
FactoryTalk Optix Studio
project:
ExampleApplication-UserSpecificPersistentSetting.zip
Prerequisites:
Application design example
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.