Ricerca
Centro assistenza FactoryTalk Optix Studio
Sessions tutorial
Configure persistent user-specific settings and buttons to close the application and shut down the system.
This tutorial assumes familiarity with the following information:
Sessions and locales
Graphic and layout objects
Retentivity storage
Dynamic links
Application examples
Develop a persistent setting specific to a user
Develop buttons for closing the application and shutting down the host system
Fornire un feedback
Hai domande o feedback su questa documentazione?
invia il tuo feedback qui
.