Develop a solution for importing translations from another project
Use OPC UA communication to import translations from another project.
NOTA:
Download the sample
ExampleApplication-ImportTranslations.zipFactoryTalk Optix Studio
project:Prerequisites:
- Create a Server project. See Create a project.
- Create a Client project. See Create a project.
MANCIA:
The Client project will import data from the Server project.
- Server project:
- Arrange the interface elements.
- Save the project.
- Client project:
- Arrange the interface elements.
- Save the project.
In
FactoryTalk Optix Studio
, select to run Server and Client projects using the client emulator to test your project. To run the project on a remote client, see Add a client device.Fornire un feedback