Add users
Add users with different locales.
Prerequisites:
Add the it-IT locale. See Add a locale language to a localization dictionary.
- In theProject viewpane, expand theSecurityfolder.
- Create two users by right-clicking theUsersfolder and selecting .
- Rename the users by hovering-over each user, selecting, and entering:
- Alice
- Jeremy
- In theProject viewpane, selectAlice.
- In thePropertiespane, set theLocaleIdsproperty value toit-IT.
Fornire un feedback