Develop a label with a localized engineering unit

Create a simple interface that displays temperature in a format that is adjusted for a logged in user locale.
Application example - Celsius degrees (it-IT)
Application example - Fahrenheit degrees (en-US)
NOTA:
Download the sample
FactoryTalk Optix Studio
project:
ExampleApplication-LocalizedEngineeringUnitLabel.zip
Prerequisites:
  1. Arrange the interface elements.
  2. Save the project.
Application design example
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.