Develop a button that changes label text
Develop a button that changes the text of a label when you select the button.
MANCIA:
You can download a sample project from:
ExampleApplication-ButtonThatChangesLabelText.zipPrerequisites
- To develop the project
- Save the project.
In
FactoryTalk Optix Studio
, select to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.Fornire un feedback