Develop a files counter
This C# solution calculates the number of files in the project folder.
Prerequisites
- To develop the project
- Create the application interface and integrate it with the NetLogic.
In
FactoryTalk Optix Studio
, select to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.Fornire un feedback