Develop a NetLogic that exports table data to CSV
This script populates table columns with data and export that data to a
CSV
file.
NOTA:
Download a sample project:
ExampleApplication-ExportTableDataToCSV.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
In
FactoryTalk Optix Studio
, select to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
MANCIA:
When you generate and export data, the CSV file is saved to the following folder:
%localappdata%\Rockwell Automation\FactoryTalk OptixEmulator\Projects\ExportTableDataToCSV\ApplicationFiles\
Fornire un feedback