Artifact Tabs

Artifact Tabs

Each time an artifact is opened, they display in tabs that can be pinned and then saved on the file system. Spreadsheets and highlighters also appear in tabs, but they are transient and cannot be pinned/saved. Datasets are pinned by default, and other artifacts are unpinned by default.
These tabs contain a tool bar with the following icons:
Icon
Description
Click the
Rename
icon to rename your tab. You can also
rename a tab by double-clicking on its name.
Click the
Save
icon to save changes to your tab.
Click the
Revert to Last Saved
icon to undo any unsaved changes and revert to the last saved tab.
Click the
Filter
icon apply filters to the data. This icon does not display for filter artifacts.
Open Preferences to change for this function.
See“Plotting Data” and Chapter 4, “Analyze Data” for more information on using plots and analysis tools.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal