- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Program syntax
This section describes the syntax for programs.
A program component defines the programs used in logic. ControlLogix and CompactLogix controllers support up to 1,000 programs.
Provide Feedback