- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Elevation view
The
Elevation
view displays all devices in the actual Motor Control Center (MCC) lineup and includes device description and the status indicators for each device. In the Elevation
view you can:- View multiple lineups simultaneously.
- Change the position of the device or section within the lineup.
- Modify the location of devices or sections within the same or different lineups.
- View status indicators for the devices being monitored within the lineup.
Provide Feedback