Module Properties dialog boxes
Use
Module Properties
dialog boxes to configure:- Generaltab properties - View the moduleTypeandVendorand configure the moduleName,Description,Slot, Minor Revision, andElectronic Keying.
- Connectiontab properties - Configure theRequested Packet Interval (RPI),Inhibit Module, andMajor Fault On Controller if Connection Fails While in Run Mode.
- Module Infotab - View moduleIdentificationandStatusinformation.
Module Properties
dialog box tabs vary based on the controller or module. Some other Module Properties
tabs include:- Powertab propertiesPower Unit Type,Voltage, and configurePower Structure Rating.
- Associated Axestab properties - Choose aServer Update PeriodandAssociated Axes.
- Configurationtab properties - Configure filter time for points.
- Setuptab properties- Choose aDrive Fileand view and edit parameter and link data associated with the drive.
- Pointstab properties - Enable Change of State for points.
- Fieldbustab properties - Launch RSFieldbus Software and view status information for Foundation Fieldbus devices.
- RSNetWorxtab properties - Use this tab to launch RSNetWorx for EtherNet/IP to view or edit the respective network, associate a EtherNet/IP project file with the respective module, and audit an EtherNet/IP network.
- SERCOS Interfacetab properties - Use theSERCOS Interfacetab to set and display the SERCOS baud rate, update rate for the SERCOS ring, and fiber optic transmit power range for the SERCOS ring.
- Backplane- View module backplane data.
Provide Feedback