- Stratix device properties
Assign an IP address to a DHCP port
Use the
DHCP Address Assignment
view to assign a specific IP address to each DHCP port. The IP address you assign is reserved for a selected port and is not available for normal DHCP dynamic assignment. The IP address must be an address from the pool specified in the DHCP Pool
field.Prerequisites
- The device is online.
To assign an IP address to a DHCP port
- On the tab for the device, selectDHCP Address Assignment.
- In theDHCP Address Assignmentview, configure these parameters as needed:
- Pool
- IP Address
- SelectSetto send the changes to the switch.TIP:You may need to enter a password in theEnter Passworddialog box.
Provide Feedback