- Stratix device properties
Configure a switch using express setup
Use
Express Setup
to configure IP addresses for the switch.Prerequisites
- The device is online.
To configure a switch using express setup
- InExpress Setup, underInternet Protocol (IP) Settings, selectManually configure IP settings.TIP:If you selectObtain IP settings automatically using DHCP, the switch automatically obtains an IP address, subnet mask, gateway address, and IP address of the Network Time Protocol (NTP) server from the DHCP server.
- Configure the rest parameters as needed:
- Physical Device IP Address
- Host Name
- Subnet Mask
- Gateway Address
- Network Time Protocol Server
- User
- Password
- Confirm
- Management Interface VLAN
- SelectOK.
Provide Feedback