- Stratix device properties
Enable an uplink port
Use the
Redundant Gateway
view to enable an uplink port.To enable an uplink port for a redundant gateway
- On the tab for the device, expandDevice Level Ring, and then expandRing X.
- SelectRedundant Gateway.
- In theRedundant Gatewayview, in theEnablecolumn, select the checkbox next to the uplink port to enable.
- SelectSetto send the changes to the switch.
Provide Feedback