- Stratix device properties
Monitor DLR status
Use the
Device Level Ring
view to monitor the status of the DLR network.Prerequisites
- You must be online and communicating with the switch.
To monitor the DLR network
- On the tab for the device, selectDevice Level Ring.
- Do one of these actions as needed:
- To view the switch and ports, selectDevice Level Ring.
- To view the ring, expandDevice Level Ring, and then selectRing X. For example, selectRing 1to view information about ring 1. There can be up to three rings.
- To view the redundant gateway on the ring, expandDevice Level Ring, expandRing X, and then selectRedundant Gateway.
- To view statistical information, expandDevice Level Ring, expandRing X, and then selectStatistics.
- To view devices on the ring, expandDevice Level Ring, expandRing X, and then selectMembers.
Provide Feedback