Device Level Ring view

Device Level Ring view

Use the
Device Level Ring
view to enable DLR on the ring and to view information about the DLR network. A DLR network is a single-fault tolerant ring network intended for the interconnection of automation devices without the need for more switches.
Use the
Device Level Ring
view to:
  • Enable DLR for up to three configured rings
  • Select the ring ports
  • View whether the switch is a ring supervisor
  • View the status of the ring
  • View whether the redundant gateway is enabled
  • View the redundant gateway status
  • View the role of the Dynamic Host Configuration Protocol (DHCP) server
  • View the status of the DHCP server
TIP:
The parameters in this view are available while online.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.