Port Diagnostics dialog box

Port Diagnostics dialog box

The Stratix device maintains counts of various features of the Ethernet protocol. Examine the counts to diagnose a problem when the link between a selected port and node is not performing as expected.
Use the
Port Diagnostics
dialog box to view the status of the link performance. You can:
  • View octet and packet counters
  • View collisions on the link
  • View errors on the link
  • Reset and clear all status counters
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.