Add Component

Add Component

Perform the following steps to add a component to the hierarchy list:
  1. Click
    Configuration
    >
    Asset setup
    from the menu bar.
  2. Click the [] icon from the asset in the hierarchy list and select [Add node].
  3. In the
    Add Node
    window, set these parameters:
    • Name
      : Provide the component name.
    • Description
      : Provide the description of the component.
    • Functional Location
      : Provide the location details.
      NOTE: Select the
      Auto generate
      check box to use the system-generated functional location.
    • Configuration Status
      : Select the status from the drop-down list.
  4. Click [Add].
    Add Component
    The "
    Component was added under the asset successfully
    " message displays.
  5. (Optional) In the
    Info
    tab, click [Edit] and perform the following actions:
    • Geographical Location
      : Provide the geographical location.
    • Contact Details
      : Provide the contact details.
    • Remarks
      : Provide the remarks.
    • Make
      : Provide the asset make details.
    • Commission Date
      : Select the commission date using the date picker.
    • Lifecycle Status
      : Select the lifecycle status from the drop-down list.
    • Files Uploaded
      : Click [Browse] to upload the files related to the asset.
    • Click [Save].
To configure
KPI
,
Sensors
, and
Advisory
tab, see Configure KPI, Configure Sensors, and Configure Advisory.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.