Asset Intelligence Dashboards

Asset Intelligence Dashboards

Dashboard Introduction
In Asset Intelligence, the dashboard section of the application is where all users can interact with the associated KPIs, Alerts, and trending data, which is all contextualized by the asset and hierarchical location.
Enables users to view the status of rolled-up KPIs according to the hierarchy. User can view the overview of each element of the hierarchy and be able to determine where they need to focus their efforts in addressing various alerts within the application.
This section of the User Manual will guide the user through each key level of the hierarchy in the application and different types of alerts, their function, and how to interact with them.
Hierarchy Dashboard Items
The following are the list of alerts available in the application:
  • KPI Alerts
  • Sensor Fault Alerts
NOTE:
As per the hierarchy configured in Asset Setup, the Dashboard displays a similar hierarchy structure only for active nodes.
NOTE:
  • No rollup KPI
    indicates that no KPI is configured as standard under the Dashboard Setup.
  • No Active Node/Asset KPI Configured
    indicates that no child node with configuration status as Active is configured or no KPI is configured under the selected node.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal