Line Charts
The line chart is represented by a series of datapoints connected with a straight line. Line charts are most often used to visualize data that changes over time.
Line Charts are used to track variations over time, which may be long-term or short-term. User can also use line graphs to compare changes over the same period for more than one group.
Provide Feedback