Post-Installation
Tasks
Once the installation
has been completed successfully, perform the following tasks to
verify the installation to configure features of the services.
- Verify User group is created successfully.
- FTA InfoPlatform Service packages installation location.
- View the installation log.
- Disable FTSecurity.
- Additional configuration steps if the service is running with a non-administrative account.
- Enable TLS.
- Verification of running services.
- Changing the service account.
- Configuring the OpcUa Provider.
Provide Feedback