View Installation Log
If the install was run using the log switch command (see “FTAnalytics InfoPlatform Installation”), User can view log information generated during the install in the file specified in the command.
Provide Feedback