Process Value Meter Dashboard
You can view the performance and energy charts of the Process value meter based on your time period selected from the date picker.
Perform the following steps to view, show/hide, and filter charts:
- Click the [
] icon from the menu bar and select
Process value meterfrom the hierarchy list.The following table provides the list of charts available by default in the dashboard:Chart TypesS.NoChart TypeDescription1Temperature details widget (Harmonized)This chart shows the maximum, minimum, and average values along with the last value and last updated time.2Trend chartYou can view the selected time period with the respective granularity on the X-axis and on the Y-axis, you can view attributes (Temperature, wind, humidity, and so on). This chart shows the process value summary. - To see the data, hover over the bar in the required chart.
- To remove the chart from the dashboard, click the [
] icon from the respective chart.
- In theDelete chartdialog, click [Delete].Delete chart dialogThe "Chart remove successfully" message displays.
- To add or show the chart in the dashboard, click the [
] icon from the top-right corner of the Process value meter dashboard.
- Select the required chart check box to add to the dashboard and click [Save].Process value meter Dashboard chart settingsNOTE: To remove the chart from the dashboard, uncheck the required chart check box and click [Save].The “Dashboard setting changes updated successfully” message displays.
Perform the following steps to change the chart time period:
- Click the [
] icon.
- Select theDateorWeekorMonthorYear, orCustomfrom the drop-down list and the calendar displays.
- Select the time period.
- Click the [
] and [
] to move forward and backward period of the selected time period respectively.
NOTE: If you selectCustomfrom the drop-down list, you need to select theFromandTodate and provide the time manually.
Related Information
Provide Feedback