Production Meter Dashboard
You can view performance and energy charts of the Production meter based on your time period selected from the date picker.
Perform the following steps to view, show/hide, and filter charts:
- Click the [
] icon from the menu bar and select
Production meterfrom the hierarchy list.The following table provides the list of charts available by default in the dashboard:Chart TypesS.NoChart TypeDescription1Total production widget (Harmonized)This chart shows the current range and past range along with the last value and last updated time.2Production data chartYou can view the selected time period with the respective granularity on the X-axis and production data on the Y-axis. This chart shows the production data summary. - To see the data, hover over the bar in the required chart.NOTE:Click the [
] icon to view the chart in the widget view and click the [
] to switch the view from widget to chart.
- To remove the chart from the dashboard, click the [
] icon from the respective chart.
- In theDelete chartdialog, click [Delete].Delete chart dialogThe "Chart remove successfully" message displays.
- To add or show the chart in the dashboard, click the [
] icon from the top-right corner of the Production meter dashboard.
- Select the required chart check box to add to the dashboard and click [Save].Production meter Dashboard chart settingsNOTE: To remove the chart from the dashboard, uncheck the required chart check box and click [Save].The “Dashboard setting changes updated successfully” message displays.
Perform the following steps to change the chart time period:
- Click the [
] icon.
- Select theDateorWeekorMonthorYear, orCustomfrom the drop-down list and the calendar displays.
- Select the time period.
- Click the [
] and [
] to move forward and backward period of the selected time period respectively.
NOTE: If you selectCustomfrom the drop-down list, you need to select theFromandTodate and provide the time manually.
Related Information
Provide Feedback