Configure OPC UA server certificates and keys
Edit the properties of an OPC UA server to configure the public certificates and private keys.
Prerequisites
- InProject view, select anOPCUAServerobject.
- InProperties, next toServer certificate file, selectBrowse.
- InSelect file:
- If the certificate is listed, select the certificate and selectSelect.
- If the certificate is not listed:
- Select
.
- Select the certificate. For more information, see Certificates and keys location.
- SelectSelect.
- Next toServer private key, selectBrowse.
- InSelect file:
- If the private key is listed, select the private key and selectSelect.
- If the private key is not listed:
- Select
.
- Select the private key. For more information, seeCertificates and keys location .
- Select theSelectbutton.
Provide Feedback