Users

Users

Users are objects in
Project view
. Assign permissions and roles to users to determine the content and interface that the user sees in the application at runtime.    
Each project has a default Anonymous user that authenticates the application session. At runtime, the session user is the user who is logged on to the application. The content and UI that appears depends on the properties and group assigned to the user. For example, the interface may change the:
  • Session locale and update the graphical interface
  • Graphic objects and information available on the interface, depending on the groups to which the user belongs
TIP: Change the default user authentication mode to allow local
Windows®
users and Active Directory users to log on to the
FactoryTalk Optix Application
. In
Project view
, select the project node and then in
Properties
, change
Authentication mode
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal