Develop a recipes management dashboard

Develop a recipes management dashboard

Create a dashboard to add, remove, and modify recipes based on a recipe schema.
The dashboard interface also incorporates additional gauges for displaying and controlling the maximum RPM and minimum throttle values of the motor.
Application example
NOTE:
Download a sample project:
RecipesManagementDashboard.zip
Prerequisites
  1. To develop the project
  2. Create and configure a recipe schema. See Configure a recipe schema or Configure a recipe schema manually.
    While creating the recipe:
    • Create a dynamic link between the 
      Target node
      property and
      ProjectName
      Model
      Motor
      .
      For more information about dynamic links, see Create dynamic links.
    • Select the
      Configuration
      MaxRevolutionsPerMinute
      and
      Configuration
      MinThrottle
      parameters.
      TIP: These parameters will be configurable at runtime.
  3. Add and configure a default recipes editor widget. See Configure a recipes editor widget.
  4. Arrange the interface elements.
  5. Save the project.
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.