- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
XY Chart
Display the value of two-dimensional variables in a graph.
Use case
Graphically represent or set machine processes, for example the cutting profile or the work area within which a machine can operate.
TIP:
You can disable the display of a pen by setting its
Enabled
property to False
.Example

Provide Feedback