- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Configure an XY chart
Configure an XY chart to visualize data.
- InProject view, inUI, right-click a container and then select .
- (optional) InProperties, set:
- Zoom. The zoom level of the chart.
- Center X. X coordinate in relation to which to center the chart.
- Center Y. Y coordinate in relation to which to center the chart.
- Key visible. Show or hide the legend of the pens.
Do any of these:
Provide Feedback