- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Add a scale line pen
Add a scale line pen to visualize the distance between two variable values.
Prerequisites
- To add a scale line pen
- Create two variables of the Number data type.For more information, see Variables.
- InProperties, next toPens, selectand selectScale line pen.
- Create dynamic links between theXandYproperties and the variables.For more information about dynamic links, see Create dynamic links.
Provide Feedback