Develop UI Generated from Model

Develop UI Generated from Model

Develop a UI populated automatically with graphical elements based on the properties of objects.
NOTA:
Download the sample
FactoryTalk Optix Studio
project:
ExampleApplication-UIGeneratedFromModel.zip
Example application
Prerequisites:
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal